Which modes can be used to adjust the motor speed?The motor speed can be adjusted by the following ways:
1. Variable resistor on the keypad
2. External analog voltage/current signal
3. Multi-function input terminals to control multi-speed control
4. Communication method by using the host controller