What should I do when the LED of a VFD-M series drive displays a 8888 or 9999 error message? The fault may occur for the following reasons:
.If the drive is still operating normally but the LED displays an error message, the LED is malfunctioning. Please replace the LED control board.
.If the drive has stopped operating, please reapply the power again. If the drive is still not operating, then it is the drive that is malfunctioning. Please send your VFD-M series for repair or replace it with a new drive.