Does Delta’s EtherCAT Interface Servo Drive ASDA-A2-E Series provide built-in regenerative resistors for both its 220V and 400V versions?For the ASDA-A2-E 220V Series, there are no built-in regenerative resistors for 100W and 200W servo drives, but servo drives with power ranges from 400W to 3kW all have built-in regenerative resistors equipped as standard.
For the 400V Series, only servo drives with power ranges from 400W to 1.5kW have built-in regenerative resistors equipped as standard, but there are no built-in regenerative resistors for servo drives with power ranges from 2kW~7.5kW.