What is the default IP address of the robot controller to make a connection with Delta’s SCARA robot?The default IP address of the robot controller is 192.168.1.1.
You must first specify the IP address of the robot controller to connect Delta’s SCARA robot and communicate with an existing network. After making the connection, the robot controller can run and control Delta’s SCARA robot to perform a series of actions according to preset programs. Data and information can be also exchanged with other devices, such as between an HMI, robot controller and PC.