Currently Delta’s CNC controller provides the pitch compensation function for one-direction compensation only. One-direction means either forward or backward from the zero point (starting point) of the machine coordinates. If the compensation direction is not set correctly, the pitch compensation function application setup will not be enabled and work normally.For setting the compensation direction, please use the compensation parameter, 1006, and set Bit 15 to determine the direction.