If users can use the constant torque when the frequency exceeds 60Hz?For general applications, the constant torque can’t be used for the frequency above 60Hz. Because the voltage and power are usually constant when the frequency is above 60Hz. When you need to have constant torque in high speed, please pay attention for choosing motors and drives.