In general, the frequency can be set to 6-60Hz (1:10). If the power still outputs when the frequency is below 6Hz?It still outputs power when the frequency is below 6Hz. According to the setting of motor temperature rise and start torque, it can output rated torque without overheat problem when the frequency is 6Hz.