When multiplying 16-bit x 16-bit or 32-bit x 32-bit on Delta’s PLC, how do I make the result of the multiplication (product) not be 32-bit or 64-bit?
You can use the PLC commands (API) MUL16 or MUL32 to simplify the multiplication. Please refer to the table below for PLC commands and the corresponding multiplication results.