How do I set up the slave station’s node ID numbers in Delta’s high-speed motion control system DMCNET?In the DMCNET, the slave station’s node ID numbers range from 0 to F. You must set the node ID number “1” in one of the slave stations. You can set the numbers of the rest of the stations randomly as long as they are not repeated.