If it is driven by the commercial power, the current will be increased when the voltage is decreased. If it is driven by the AC motor drive, will the current be increased when the frequency and voltage are decreased?When the frequency is decreased, the current will be increased with the same output power. However, the current will be almost the same for the constant torque.