1. Calculate the supporting motor speed using the equation below:
Speed = 120*frequency/number of poles for motor
2. The AC motor drive has two RS485 communication ports as indicated in the diagram below (Channels 1 &2).
a. Channel 1: One common port for RJ45 and RJ11
b. Channel 2: Two RJ45 ports and a terminal
c. Communication protocol for channel 1 is 19200, 8, N, 2
d. The default setting for the drive station is 1 and the PLC station is 2.
According to the C2000 user manual Chapter 16-2, the default setting for the PLC communication protocol is 7,N,2 ,9600; the station is 2. The user may change the PLC station from Pr.9-35, but the address should not be the same as the drive’s address in Pr.9-00. The communication protocol can also be changed by Pr.09-04.