What is vector control?In the AC motor, rotor generates flux by the current from stator winding induction. There are two elements in stator current, one affects flux and the other affects the output torque of motor. The flux vector can control these two elements individually so that the speed and torque can be controlled.