How should I do when the actual speed is different from the desired speed?When the AC motor drive is controlled by the open loop, the motor speed will be varied within ±5% X rated slip. You can use the AC motor drive with the PG feedback function when the accurate speed is required.