Delta has developed the Woodworking Electronic Saw Machine Suite, which provides abundant and diverse functions. One of the useful and critical functions is the optimized composing algorithm that significantly enhances board utilization and eliminates manual operation.

On the control layer, Delta’s Industrial PC IPC Series transmits data to the Programmable Logic Controller DVP Series. The PLC connects with the AC Servo System ASDA-B3 Series and Standard Compact Drive MS300 Series to accomplish high-precision control.