Clients can manage real-time information with Delta’s human machine interface (HMI) 10-inch DOP-B series.

Delta’s DMV Series achieves position inspection for automotive production lines.

Two sets of DMV Series are installed respectively on the right and left side of a working station. They ensure the locating pins insert into car chassis correctly by highlighting and inspecting the connection parts of locating pins and car chassis. They can detect the same misalignment and sound an alarm with a same procedure.

There are no black dots inside the green box when a car’s position is normal. When a misalignment occurs, black dots exceed the preset location and range on the interface of the DMV Series, and the system sounds an alarm.

Position of DMV Series cameras on the production line