2/24/2022

Delta’s New CNC Controller NC5 Series Boosts Smart Machinery at TIMTOS x TMTS 2022

Delta Demos Next Generation Cloud and On-premises Integration for Smart Manufacturing

In 2020 and 2021 both TIMTOS (Taipei International Machine Tool Show) and TMTS (Taiwan International Machine Tool Show) canceled their onsite exhibitions due to the COVID-19 pandemic as Taiwanese machinery exports remained at a low ebb. Recently, the industry glimpsed the light of recovery and was ready to welcome the largest-scale exhibition since the coronavirus outbreak. The organizers of TIMTOS and TMTS have joined forces for the first time to hold the "TIMTOS x TMTS 2022" exhibition from 2/21 to 2/26. The show is attracting visitors from a wide range of fields to come and explore how the machine tool industry is aligning with smart manufacturing.

After the long wait, Delta has focused on the theme of cloud and on-premises integration for smart manufacturing at this large machine tool industry event. Delta is presenting exhibits in the fields of Smart Machining Solutions x Machine Networking, CNC Industrial Applications x Peripheral Applications, and Smart Machines. Moreover, Delta has taken the opportunity to debut its next generation High-performance General CNC Controller NC5 Series. Delta is also exhibiting one-stop smart machining solutions integrating the NC5 Series and various industrial automation products and software systems that help customers develop business opportunities in smart manufacturing.

Numerous potential customers and media have visited Delta’s booth and exchanged ideas for the machine tool industry. There are also live demos in cooperation with machinery partners that received much attention. Among these, the most popular demo machine is the 5-axis Machining Center. With the integration of the new OPEN CNC controller NC5 Series and Articulated Robot DRVA4LC, it has impressed visitors with its RTCP features and the capability to connect to the IT layer with the Equipment IoT Platform DIALink for empowering machine tool production with intelligence.

To explore more about smart machinery, you are welcome to visit Delta’s booth (Q314, 1F, Hall 2, Nangang Exhibition Center) at TIMTOS x TMTS 2022 on 2/26, the last day of the exhibition, or visit Delta’s virtual booth at: http://iacommunication.deltaww.com/event/MachineToolTPE/index.html#2_4_tc.

News Source:IABG MKT