How should users set up the SMS function in the Industrial Energy Management System DIAEnergie?
1. Execute DIAEnergie quick Installation
2. Install the driver based on the SMS device model
3. Go to Device Manager to check out the status of the SMS modules’ communication protocols. Please select an AT COM Port of your choice (COM6 or COM7 as shown in the image below) to set up DIAEnergie.
4. Set up a SIM card code via the SMS device (Note: Inputting an incorrect code may lock your SIM card by carriers. Please be sure of the code before setting). Install the SIM card at the back of the SMS device. DO NOT connect the device to a computer until both the SIM card and SMS device’s COM Port setup are complete.
5.Open DIAEnergie to set the up system / alarm / SMS device. Check the Y (Yes) option for initiation. In the COM Port column, select the previously set up AT COM Port of the SMS module’s communication protocol. In the SIM PIN column, input the SIM card code if there is one, or leave the column blank.
6. Connect the SMS device with the DIAEnergie connected computer to complete the SMS message setup. In addition, simply check the “SMS” option in the edit window for alarm notification setup.
● Software Requirement:
Minimum supported version of the DIAEnergie: 1.7.4.0
● Supported Devices:
GTM-203M-3GWA (http://m2m.icpdas.com/gtm-203m-3gwa.html)
GTM-204M-4GE (http://m2m.icpdas.com/gtm-204m-series.html)