How do I set up the data exchange function of Delta’s programmable logic controller (PLC) DVP-SE Series?
Step 1: A maximum of eight sets of data exchange links can be set up via the DCISoft Ethernet configuration software for the DVP-SE Series PLC.

Step 2: In the Data Exchange tab, click Enable Data Exchange, then choose “Program Control” in the drop down list box.

Step 3: The CR#13 register is the data exchange trigger for the execution of data exchange. Use the From/To station to transmit data to CR#13. The Ethernet port for From/To station in DVP-SE Series PLC is K108.
Through this process, the user can execute the data exchange function in DVP-SE Series PLC.