In the current Industry 4.0 revolution, there is an increasing demand for machine to machine communications. Does Delta’s CNC solution provide any communication protocol to support data exchanges in the information level or with other devices?
Delta’s CNC solution supports RS-485 (MODBUS) and Ethernet communications.
.When the Delta CNC controller works as a Master, it supports MODBUS communication with other Slave devices such as The Delta Power Meter DPM Series, Delta Temperature Controller DTB Series, Delta Machine Vision System DMV Series and Delta SCARA Robot.
.When the Delta CNC controller works as a Slave, the Master device is able to acquire data through the MODBUS address as below,

.Communication via Ethernet: Users are able to edit the API command supported by Delta’s CNC controller for data exchanges.