What is Auto Tuning?

Auto Tuning is to measure the motor parameters automatically, including no-load current, stator resistance, rotor resistance, stator inductive reactance, rotor inductive reactance, etc. These parameters are used to calculate the torque estimation and slip compensation. With auto tuning, it can get accurate speed without encoder.