可以用新的DOP-B08S515系列取代DOP-A75CSTD系列的人機介面嗎?硬體方面可以直接取代,但DOP-A系列跟DOP-B系列的操作軟體不同,目前還無法直接轉換。雖然A75CSTD系列已經下市,但其操作軟體仍然支援Windows XP及Windows 7 (32位元)作業系統。如果需要轉換,先以支援A75系列的ScreenEdit 1.05.78版本軟體打開操作用.dop檔案,在機種欄位選擇較高階的DOP-A80THTD,按下確定後儲存檔案,再以新版人機介面用的操作軟體DOPSoft開啟此檔,開啟後會跳出欲更改的機種型號及是否需自動調整尺寸的對話框。因DOP-B08系列沒有輔助鍵,若原先有使用輔助鍵功能,轉換時就須移除。