Greening intelligence: Charting the future of sustainable AI
The coming surge in
AI sustainability
- but are leaders ready?
AI 永續浪潮來襲,你準備好了嗎?
Artificial intelligence is revolutionising business, but at what cost? While AI offers enormous benefits, its environmental impact is becoming impossible to ignore.
人工智慧正顛覆全球商業模式,但代價是什麼? AI 帶來巨大效益,但其環境衝擊也愈來愈難以忽視。
  Based on a global survey of 608 senior executives - 41% of whom are C-level - the Economist Impact’s latest research reveals that businesses are approaching a critical inflection point.
《 Economist Impact》針對全球608位企業領袖(41%為C-level)的最新研調指出,企業正走到關鍵轉捩點。
AI boom rising
AI 崛起
儀表板背景圖
46%
0%
91% of executives predict that AI will be 'important' in 12 months, up from just 47% today
91% 企業領袖認為 AI 將在一年內變得至關重要,遠高於現在的47%
AI boom rising
AI 崛起
91% of executives predict that AI will be 'important' in 12 months, up from just 47% today
91% 企業領袖認為 AI 將在一年內變得至關重要,遠高於現在的47%
 
44% of the companies say that AI energy efficiency is important today but will increase to 78% in the next 12 months
全球對 AI 能源效率的關注,將在一年內從 44% 提升至 78%
Companies are recognising the need to balance AI innovation with sustainability concerns, as the energy demand for AI is surging. However, organisations do not see a “silver bullet” solution.
面對 AI 能源需求飆升,企業開始重視創新與永續的平衡,然而多數組織仍未找到一勞永逸的解方。
 
42% of AI suppliers adopt edge computing to improve efficiency
42%的AI供應鏈採用邊緣運算提升能源效率
AI-driven innovation offers great potential to advance sustainability. Edge computing and hardware infrastructure are central to sustainability efforts.
AI 創新可望推動永續發展,邊緣運算與硬體基礎架構是實現的關鍵。
 
38% of AI suppliers identify power and grid resilience as the top sustainability challenge
38%的 AI 供應鏈認為電力與電網韌性是永續的主要挑戰
Power systems must contend with increasing climate volatility, ageing infrastructure and rising energy demands.
電力系統正面臨氣候變異加劇、基礎設施老化與能源需求攀升等多重挑戰。
Sustainability hurdles limit progress
阻礙永續 AI 推進的挑戰
 
Events
活動花絮
(左至右)品牌長郭珊珊、董事長暨執行長鄭平與Economist Impact亞太區科技與創新總編輯Charles Ross合影
鄭平董事長於AI趨勢論壇分享台達的科技解方,呼應Economist Impact報告中點出的永續AI挑戰。
Economist Impact亞太科技創新總編Charles Ross分享全球永續AI的產業洞察。
AI趨勢論壇全場滿座,吸引約四百人參與,廣受迴響。
鄭平董事長於演講後參與座談,與Google 台灣區前董事總經理簡立峰與前科技部長陳良基等產學界名人交流觀點。
鄭平董事長也於法說會上向投資人及媒體朋友分享報告的重點觀察。