<% Response.Charset="UTF-8" Session.CodePage="65001" %> Delta Feature Story
Feature Story

A Green Energy Pioneer under the Brilliant Ako Sun

Upon exiting the Banshu-Ako JR station, we have arrived at Ako City in Western Japan. The freshness of the air is a strange yet familiar feeling. Bordering the Seto Inland Sea, the location is approximately two hours from Osaka. The rural location has preserved rustic elements of nature and culture. The Chikusa River flows past the city, once renowned as one of the cleanest rivers in all of Japan. The river’s waters are still crystal clear even today. The loyal samurai spirit of the 47 Ako Ronin protecting their master more than 300 years ago has been passed down through history in The Fall of Ako Castle, which was based on historical events……



Sharing Green Experience



Ever since the tragic earthquake and nuclear power plant accident hit eastern Japan in 2011, a well-balanced energy combination and supply system have been a major social concern. As I wondered how we could contribute to meeting this challenge with our expert knowledge and technology in power management, it came to my attention that there was a suitable location for building a mega solar plant in Ako City in western Japan.

My intention was not to build conventional type of mega solar plant but to realize a new generation that would blend well with the natural geography of Japan where most available land is hilly. We chose the distributed solar generation system as the best solution for not disturbing the natural contours of the land and for maximizing power generation efficiency...



C.H. Ko / Delta Japan




Sharing Green Experience

Ever since the tragic earthquake and nuclear power plant accident hit eastern Japan in 2011, a well-balanced energy combination and supply system have been a major social concern. As I wondered how we could contribute to meeting this challenge with our expert knowledge and technology in power management, it came to my attention that there was a suitable location for building a mega solar plant in Ako City in western Japan.

My intention was not to build conventional type of mega solar plant but to realize a new generation that would blend well with the natural geography of Japan where most available land is hilly. We chose the distributed solar generation system as the best solution for not disturbing the natural contours of the land and for maximizing power generation efficiency...

C.H. Ko / Delta Japan





Numbers Talk

The Delta Ako Energy Park has outstanding numbers:


Numbers Talk

The Delta Ako Energy Park has outstanding numbers:


4,900,000

The Delta Ako Energy Park is expected to generate approximately 4,900,000kWh of clean energy per year to create sustainability.

96,000

The park takes up an area of 96,000m2 of recycled forest land, while taking advantage of geographical features.

17,256

The park’s PV system uses 17,256 solar modules of 265Wp.

185

The entire system links 185 units of Delta’s RPI-M series string PV inverters, which include 175 sets of 20kW Delta RPI-M20A and 10 sets of Delta 50kW RPI-M50A high-efficiency inverters, and feature strong enclosures to withstand adverse weather conditions.

930

The expected electricity generation per year of the Delta Ako Energy Park is equivalent to the electricity consumed by 930 local households annually.






Green Background

Delta’s first proprietary large-scale solar plant, Delta Ako Energy Park, was completed and put in service in January 2016. This power plant is located in a mountainous area of Ako City in Hyogo, Japan. The new plant is equipped with a capacity of 4.6MW and takes up an area of 96,000m2. One of its main features is a distributed PV system built with medium-size solar inverters in response to the irregular terrain and to improve the overall power generation efficiency.

As the largest class mega solar plant with a distributed system connecting to an extra-high voltage (33,000V) grid in Japan, Delta Ako Energy Park is expected to generate approximately 4,900,000kWh per year, which is equivalent to the electricity consumed by 930 local households annually. According to the Renewable Energy Special Treatment Act of Japan, the power generated by the Delta Ako Energy Park will be sold entirely to the power company, and it has helped create a new business model for Delta. The completion of the Delta Ako Energy Park is also a milestone for Delta’s active focus on renewable energy, providing clean energy to help create sustainability for the environment and cities.


Dictionary