4/29/2019
Delta Presents Complete Industrial Automation Solutions for the Turkish Market at WIN EURASIA 2019
Delta recently participated in the WIN EURASIA 2019 show at the Tüyap Fair Convention and Congress Center in Istanbul, Turkey from March 14th to 17th. At the event, Delta presented integrated industrial automation solutions and products, ranging from AC motor drives, controllers, AC servo systems, CNC solutions, HMIs, industrial Ethernet products to industrial robots. Delta displayed a variety of live demos of actual applications and functions of the products. Highlights included the Delta Compact Drive M300 Series, Multi-axis Motion Controller DVP-15MC Series and Packaging Solution. Delta showcased its determination for developing the Turkish market.
WIN EURASIA is the most significant international industrial exhibition in Turkey. This year, WIN EURASIA gathered 1,300 exhibitors from 20 countries around the world and more than 70,000 visitors. Situated at the hub of Europe and Asia, the Turkish market is prosperous and full of opportunities. Delta utilizes its strong R&D capabilities and years of experience to present integrated industrial automation products and solutions that meet local market demands, including:
• Compact Drive M300 Series: The M300 Series is Delta's latest AC motor drive product. It offers three types: the High Performance Compact Drive MH300 Series, the Compact Drive MS300 Series, and the Basic Compact Drive ME300 Series. Inheriting the excellent drive capability of Delta's AC motor drives, the M300 Series features a compact design, excellent performance, and high expandability. The Screw-less terminals enable easy installation and maintenance. With the built-in USB port, users can duplicate parameters quickly to enhance efficiency.
• Multi-axis Motion Controller DVP-15MC Series: The DVP-15MC Series is a multi-axis motion controller with CANopen communication that offers built-in motion control commands for users. The DVP-15MC is capable of controlling up to 24 real axes and supporting multiple single-axis and multi-axis motion commands. At the booth, Delta displayed the E-CAM functions of the DVP-15MC with a live demo. With a variety of built-in communication interfaces, the DVP-15MC can be used as a master controller to connect other field devices in a complete system structure without additional communication modules.
• Packaging Solution: This solution adopts the Hot Swappable Mid-range PLC AH Series as master controller, connecting the AC Servo Drive ASDA-A2-E Series to control the axes via EtherCAT communication. The modular controller AH Series offers various modules for users to choose from and expand functions. The ASDA-A2-E Series supports EtherCAT communication. Its built-in rotary cut function enables stable and precise packaging work. The solution also features the Photoelectric Sensor PS-R Series, Standard Multifunction Pressure Sensor DPA Series, and Intelligent Temperature Controller DTK Series. With compact and stable smart sensors, Delta provides customers with an outstanding automated packaging machine solution.
Not only is the economy in Turkey growing rapidly, it is also one of the top machine exporting countries in the world. Currently, the gross output (GO) of the Turkish industrial automation industry is 1 billion USD. Thanks to its excellent location as the bridge to Europe, North Africa, Central Asia and Middle East, Turkey has great potential of business development. Delta presented an outstanding lineup of efficient industrial automation solutions and products at WIN EURASIA 2019, as it continues to develop the market, and establish its brand and “Automation for a Changing World.”