6/24/2016

Event Review: Delta's Smart, Innovative Industrial Automation Products and Solutions Exhibited at SPS/IPC/DRIVES/ITALIA 2016 in Italy

Delta Industrial Automation (IA) attended the SPS/IPC/DRIVES/ITALIA 2016 exhibition in Parma, Italy from May 23rd to 25th. Focusing on markets in Italy and Europe, Delta IA presented a full range of automation products and solutions, and highlighted its IP54 protection rated High Durability Vector Control Drive CFP2000 Series and Internet Cloud Service Platform DIACloud, as well as its Energy-saving Elevator Solution and Multiple Water Pumps Control Solution.

SPS Italia originates from the German fair SPS/IPS/DRIVES/NUREMBERG (SPS Nuremberg), which has been the leading industrial automation event in Germany and Europe for over two decades. To effectively promote the Delta brand and products, Delta IA attends SPS Italia in May, and showcases at SPS Nuremberg in November every year.

Since the 1950s, Italy's main economic development has evolved from agriculture to industry. After years of progress, Italy is now listed in the world's top 10 economies and it is the 6th largest food exporter. Italy's clothing, household appliance, automotive and chemical industries have also boomed in recent years.

Aware of the needs of the manufacturing industries of Italy's local markets, Delta showcased many automation products during this year's SPS Italia, including AC motor drives, servo drives, PLCs, HMIs, and automation products and services for smart manufacturing. Delta's display focused on:

.Industry-specific fan/pump drive CFP2000 Series is Delta's brand new high durability Vector Control Drive for fan and pump applications. Featuring a built-in EMC filter, DC chokes, Real-Time Clock (RTC), and BACnet, the CFP2000 Series provides the best solution for the special needs of the HVAC industry. The IP55 model features highly effective protection against dust and water in harsh environments.

Delta's Internet Cloud Service Platform DIACloud provides big data storage and management for remote monitoring by users. DIACloud is able to collect real-time facility operation data with Delta's supervisory control and data acquisition (SCADA) system DIAView, and energy consumption information and industrial energy management system (IEMS) DIAEnergy. It can also acquire and preserve operational information when connected to an Enterprise Resource Planning (ERP) system and Manufacturing Execution System (MES), manufacturing facilities and factory facilities. With data saved and managed, DIACloud allows users to access and remotely monitor real-time operational information via PCs and mobile devices, providing a fast and convenient real-time remote monitoring solution for smart manufacturing.

Delta also launched its best-selling energy-saving solutions in Europe, including:

.Multiple Water Pumps Control Solution performs pump management with several control modes, such as pressure, temperature or constant level, and provides a configurable hardware and software system to control up to four pumps. The solution is suitable for water pumps in HVAC systems, water treatment, and other applications that require multiple pump control. In addition, the solution supports remote connection via 3G router and Delta's internet cloud service. Users can remotely maintain and manage the whole system through Windows, Android, and iOS systems.

.Elevator Solution saves up to 40% in energy for elevator systems through power regeneration provided by Delta's Power Regenerative Unit REG2000 Series. The elevator system also delivers smooth rides and door open/close with Delta's Elevator Drive ED Series and Door Control Drive VFD-DD Series.

With products and solutions well-suited for local customers, Delta's display at SPS Italia 2016 attracted the attention of many machine makers, component suppliers, system integrators and customers from various industries. They came to Delta's stand and asked about Delta's products and solutions, bringing excellent business opportunities and making the exhibition a great success.

Delta has built a complete sales and service team in Italy, and we are ready to provide better, more immediate and comprehensive sales and after-sales service to customers in Italy. In the future, Delta will continue to offer customers in Italy and Europe more innovative, green and value-added automation products and solutions.

News Source:IABG MarCom