Please enter your profile and select news type(s) you want to subscribe to. We’ll start delivering Delta news via email alert after your account being activated.
 
Press Releases
  2019/03/28  
  Delta’s Industrial Automation Solutions for Digitalized, Visualized and Integrated Smart Manufacturing Unveiled at Hannover Messe 2019
 
   
   
Delta is demonstrating its enhanced spectrum of solutions for the digitalization, visualization and integration of smart manufacturing at Hannover Messe 2019 from 4/1~5. An impressive 220-inch video wall at Delta’s booth features the newly-launched Digital Factory Monitoring Solution, which integrates a series of software platforms developed by Delta to determine in real-time the status of manufacturing processes, equipment and energy consumption. The new DIAStudio integrated engineering software enables an all-in-one platform to select models, program and set up PLCs, HMIs, drives and more, allowing for effective and time-efficient machinery systems development. Delta’s new CODESYS-based Motion Control Solution, matched with a Delta SCARA robot, will also be a highlight of our showcase.

Andy Liu, general manager of Delta’s Industrial Automation Business Group, indicated, “The development of smart manufacturing is a major pillar of Delta’s long-term strategy. By leveraging its commitment to innovation, automation hardware-software integration capabilities, and energy-efficient manufacturing expertise, Delta develops comprehensive platforms that help our customers’ production facilities reach the smart manufacturing standard. By utilizing Delta’s smart manufacturing solutions in our own PLC production lines, we are targeting an improvement in production capacity by approximately 70%, a reduction in production area by 35%, and at least a threefold increase in direct labor per-worker average productivity.

To foster the smart manufacturing megatrend, Delta is launching its new Digital Factory Monitoring Solution, an IIoT-based platform in which various Delta software systems converge to facilitate a 360-degree monitoring view of manufacturing and factory operations, such as production equipment data collection (DIAMMP Manufacturing Management Platform), factory facility operation (DIAView SCADA system) and overall factory energy consumption (DIAEnergie). Visitors at Delta’s exhibition booth will witness the cutting-edge automation, digitalization and visualization qualities of the Digital Factory Monitoring Solution in a 220-inch video wall.

The DIAStudio integrated engineering software is an all-in-one system designed to simplify and reduce the time required for the setup process in machinery systems. Tasks such as product (Delta’s HMIs, PLCs, servo drives and motors, AC motor drives) selection, PLC programming, quantitative parameter setting, machine tuning and HMI integration can all be executed smoothly with DIAStudio’s key tools:

• DIASelector: A PC and APP-based (Android) mechanism to select the specific elements in the machine system.

• DIADesigner: After users have exported the model selection information out from the DIASelector, they can use the globally-adopted CAD software EPLAN for project planning and configuration, and then import the configured data to the DIADesigner to execute the programming, parameter settings, tuning and management.

• DIAScreen: A tool to achieve tag sharing between PLCs and HMIs/text panels.

Following Delta’s cooperation with CODESYS, announced last November at SPS-IPC Drives Nuremberg, Delta is showcasing its brand new CODESYS-based Motion Control Solution and the upcoming PLC-based Extended Motion Controller DXMC series at Hannover Messe 2019. The former solution boasts compliance with IEC62231-3 standards to enable user-friendly integration of PLCs, HMIs and motion controllers into one single platform while also supporting EtherCAT protocol to simultaneously control field devices. The latter solution enables synchronous multi-axis motion control with an optional CODESYS SoftPLC in either standard type or panel type (7 inches / 10inches). Just as the earlier version PC-based Motion Controller AX864E series, the DXMC can control up to 32 axes (standard type) / 8 axes (panel type). Visitors at our booth will also experience Delta’s industrial robots working on a CODESYS environment to provide user-friendly and highly productive operations.

Other highlights from Delta’s Industrial Automation Solutions presented at Hannover Messe 2019 include:

• The Vector Control Drive C2000 Plus series is a heavy-duty drive based on the architecture of the highly successful drive C2000 series. With 460V models reaching up to 560kW rated power overload capacity, it offers the best possible stability and performance of speed and position control for both sensor and sensorless types of synchronous and asynchronous motors, which are commonly used in heavy-duty and constant torque applications in the fields of food and beverage, metals, chemicals, plastics, and rubber. The C2000 Plus supports a wide range of protocols and built-in PLC functions for up to 10k steps.

• Delta’s new Multi-Loop Temperature Controller DTM series is designed to provide highly accurate temperature-based control in advanced and complex applications. Its modular and scalable design includes the host, up to 7 temperature modules, and up to 8 I/O extensions, thus, capable of supporting up to 64 points of temperature control. By functioning with widely used protocols such as RS-485 and Ethernet, it can offer temperature control for more than 1,000 points. The DTM series also boasts complete isolation between channels to facilitate fast and stable information transmission, which are critical requirements in glass bending, plastic molding and ceramic plating machines.

• The newly-launched Multi-Axis Motion Controller DVP50MC series supports CANopen communication protocol and EtherCAT motion control protocol to control a maximum of 24 axes. The DVP50MC not only offers simple single motion control instructions such as speed, torque, homing and position, but also provides multi-axis motion control instruction for electronic gear, electronic cam, rotatory cut as well as G-code. This innovative motion controller has built-in Ethernet and Profibus network interfaces to reduce additional connectivity costs and to allow for a broader application spectrum, including machine tools, beverage injecting machines, printing machines, and electronics manufacturing.

Other total solutions exhibited this year offer substantial benefits to applications such as woodworking, packaging, elevators, water treatment and more. Visit our event website at: http://www.deltaww.com/event/HM2019/, or contact your local service team for more information. We look forward to seeing you at Delta stand A57, Hall 11, at Hannover Messe 2019 from April 1st to 5th, Germany.

Hannover Messe 2019
Date: April 1st – 5th, 2019
Venue: Hannover Exhibition Grounds, Hannover, Germany
Delta Booth: Stand no. A57, Hall 11
Delta at Hannover Messe: http://www.deltaww.com/event/HM2019/
Hannover Messe 2019: http://www.hannovermesse.de/home 
Delta welcomes you to Hannover Messe 2019 at stand no. A57, Hall 11 , from April 1st ~ 5th
News Source: IABG Marcom
     
   
 
  Delta Electronics' Board of Directors Approved Purchase of L...
  Delta Achieves ENERGY STAR® Sustained Excellence Award for ...
  Delta Electronics’ Consolidated Sales Revenues for March 201...
  Delta Demonstrates IoT-based Smart Green Solutions to Enable...
 
 
 
 
 
 
Information
Privacy Policy Data Collection
Terms of use Contact us
 
Follow Us
© 2019 Delta Electronics, Inc. All Rights Reserved.