12/30/2016
Event Review: Delta Exhibits at Rajkot Machine Tools Show 2016 and ALUCAST 2016 to Promote Industrial Automation in India
Delta Industrial Automation (IA) recently participated in two exhibitions in India: the Rajkot Machine Tools Show 2016 (November 23 - 26) in Gujarat and the ALUCAST 2016 show (December 1-3) in Bangalore. With the aim of fulfilling market demand in India, Delta IA showcased a complete line of industrial automation products and solutions with high efficiency and reliability. Display highlights from both exhibitions include Delta's CNC controller, Hybrid Energy Saving System for injection molding machines, industrial power supply and power quality solutions which received positive feedback from many visitors.
With rapid growth of its manufacturing industry, India is developing the domestic machine tool market to replace its dependence on imports. To address this market trend in India, Delta showcased diverse industrial automation products and solutions at both exhibitions. The displays included:
•CNC Solution
Delta's CNC Controller NC300 Series features high-speed and high precision for multi-tasking via intuitive human machine interface (HMI) and CNC Soft software with user-friendly setup support and operation. It is particularly suitable for the high-speed tapping, engraving and milling processes. In addition, Delta's CNC solution precisely executes mold manufacturing or advanced gantry control for efficiency and productivity enhancement.
•Hybrid Energy Saving System for injection molding machines
Plastic products are often everyday necessities made with injection molding machines. By employing the Delta Hybrid Energy Saving (HES) System to precisely control and adjust the speed of molding pressure and flow needs of the manufacturing processes, the HES saves up to 60% in energy consumption compared to traditional quantitative pump hydraulic systems and reduces oil usage by 50% to 60% with enhanced production efficiency and low maintenance costs.
• Power Quality Solution
This solution includes Delta's Active Front End AFE2000 Series which can achieve more than 95% power generation efficiency and power factor improvement. By converting regenerative energy into electricity for energy feedback, the AFE2000 reduces energy consumption and can provide Delta's AC motor drives with quick and maximum braking for operations in the machine tools and lathes industries.
• Industrial Power Supply
For India's increasing local demand in industrial applications, Delta offers industrial power supplies with high stability and efficiency including DIN rail, panel mount, and open frame models. Delta's industrial power supplies can be applied at a wide temperature range from -20°C to +75°C and made to withstand harsh industrial environments with its safety protection functions, serving as a basic component in the automated production process.
The Rajkot Machine Tools Show 2016 is considered a major local machine tool exhibition in India, while the ALUCAST 2016 is noted as the nation's biggest industrial platform for aluminum casting. Both events attracted many visitors from the industrial fields, and Delta was able to introduce its diverse automation products and solutions for simple processing and high efficiency to local manufacturers. Delta continues to explore more business opportunities with our customers for the near future.