5/29/2012
Delta Innergie@@s PocketCell Wins 2012 Computex Best Choice Award
Taipei, Taiwan, May, 29, 2012 – The new PocketCell rechargeable battery bank from Delta Electronics' consumer brand Innergie has won the 2012 Computex Best Choice Award. The award is the highest honor presented at Computex Taipei, the largest ICT trade show in Asia. The Innergie PocketCell is an innovative and compact rechargeable battery bank that features a 3-in-1 charge & sync cable, integrated Apple connector, Micro USB, and Mini USB tips. The PocketCell can charge or provide extended power to virtually any mobile device such as iPads, iPhones, iPods, HTC, Samsung, and BlackBerry, Android smart phones, media players, and more than 10,000 other portable devices, as it fulfills Delta's brand concept "Smarter, Greener, Together".
The senior director of Innergie, P.S. Tang, said, "The PocketCell is compact and lightweight at 72 grams, and its 3,000 mAh rechargeable battery bank can extend the operating hours of mobile devices. For instance, it can extend the iPhone's talk time to more than 25 hours." The PocketCell not only has a built-in smart chipset and 2.1 amp fast-charging USB port to fast charge and recharge mobile devices, but it also has built-in power protection systems to ensure safety, including: over current protection, over voltage protection, overheating protection, over power protection, and short circuit protection.
The Innergie PocketCell battery bank comes in a stylish one-piece design with an elegant piano-lacquer finish. For energy saving the built-in Auto Sleep Mode turns the power off after 10 seconds when not in-use.
The Innergie PocketCell is exhibited at Delta's Booth number L0631a located in the Nangang Hall 4th floor at 2012 Computex Taipei.