1/29/2014

Delta unveils its latest display technologies at ISE 2014, Amsterdam

Amsterdam, NL, January 29, 2014 – Delta, a leading provider of display technologies, will exhibit its state-of-the-art display solutions at ISE 2014, Amsterdam from February 4-6, 2014. Visitors will experience the distinctive and diversified features of our display innovations. Delta's Ultra Slim Series Video Wall will showcase its advanced lightweight design and suitability for smart control rooms while our vision control systems, DVCS and MiNiCON will demonstrate their value-added features on LCD Video Walls for control rooms and non-control room applications. The new, compact and lightweight WideXtreme megapixel display will highlight its remarkable functionality for diverse applications.

A new Ultra slim Series Video Wall featuring a noteworthy depth < 535mm, lightweight design, super-efficient LED light engines, redundant power supplies, auto alignment and auto color calibration is particularly suitable for today's smarter control rooms. Delta's latest LED display product, a 4mm Pitch indoor LED wall offers an ideal solution for large format indoor full-color, full-motion dynamic, life-like content display and overcome the challenges of viewing distances for large audiences for permanent display structures as well as temporary ones.

All the DLP and LCD Video Walls are powered by Delta's DVCS and MiNiCON (Embedded Vision Control System) control systems offering the visitors a chance to touch and feel their advanced functionality. The IP-based, highly expandable DVCS (Distributive Vision Control System) supports over 10,000 sources and displays while the other control system available, MiNiCON, is a fully embedded video wall controller that adds significant value to the video wall functionality by delivering up to 60fps performance and stability regardless of the number of inputs and outputs.

Delta's WX display solutions will demonstrate how multiple users can access and share content on a super-large digital canvas simultaneously by using their own mobile devices over an existing WiFi or Ethernet network.

ISE is Europe's largest tradeshow for professionals in AV and electronic systems industry. Visitors can experience Delta's display capabilities for indoor messaging, control rooms, collaboration and visualization markets at ISE 2014, Hall 9, Booth D111.

News Source:Corporate Communications