2/24/2009
Delta Rolls Out Innovative, Advanced Renewable Energy Solutions at PV Expo 2009 in Tokyo
Taipei, February 24, 2009—Long dedicated to innovation, energy efficiency and environmental protection, Delta Group is presenting a variety of innovative and advanced renewable energy solutions at the upcoming 2nd Int'l Photovoltaic Power Generation Expo 2009 (PV Expo 2009), Asia's largest PV Expo, held in Tokyo, Japan. Delta Electronics, Inc., Delta Energy Systems, and DelSolar Co., Ltd., will showcase a wide range of renewable energy applications including high concentrating PV modules, advanced solar cells, and highly efficient PV inverters with industry-leading power output at Booth No. PV6-23, West Hall 1.
Mark Ko, president and chief operating officer of Delta Electronics, Inc., said, "This is the second year Delta Group has demonstrated our capabilities for developing a full portfolio of world-leading PV system solutions at PV Expo in Japan. Hundreds of companies from around the world are gathered there to display cutting-edge PV technologies and products. Delta is honored to be there to share our experience, our alternative energy solutions and, most importantly, our vision for a cleaner world."
Delta's Featured Products at PV Expo 2009
High Concentrating Photovoltaic (HCPV) System Solution – Delta Electronics, Inc
http://www.delta.com.tw/product/cp/cpv/cpv_main.asp
Since 2005, Delta's strategic partnership with Spectrolab has developed high quality concentration photovoltaic receivers for their high efficiency multi-junction solar cells. Two standard cell assemblies (CA0505 and CA1010) are already available to the market and are used by many CPV module makers worldwide. Delta's first generation MA0505 high concentrating photovoltaic (HCPV) module uses Spectrolab's 37% high efficiency multi-junction solar cell and has constantly achieved over 25% efficiency in production. The HCPV module has passed the 13 testing criteria of IEC62108 and Delta has shipped over 4,000 units to customers.
Besides the HCPV module, Delta will also debut its own tracker and sensor products during PVEXPO to offer complete system solutions to customers. Meeting strict requirements for operating in harsh environments, Delta's tracker has sensors with anti-jamming functions for cloudy conditions and it is able to achieve a high precision tracking accuracy of 0.05 degrees. All Delta products are RoHS compliant.
Highly Efficient Central Inverter System–Delta Energy Systems
http://www.solar-inverter.com
Delta Energy System is presenting a prototype of its new highly efficient CI 100 Central Inverter, which offers maximum flexibility, user-friendliness and high reliability due to its modular system concept. The modular central inverter system has up to nine inverter modules, which can provide a power output of 11 kW to 100 kW. The transformer based system has a peak efficiency up to 95.6%. With the CI 100 Delta is meeting the demands of the market in terms of flexible inverter solutions with higher power ratings.
Advanced c-Si Solar Cells and Solar Modules – DelSolar Co. Ltd.
http://www.delsolarpv.com
With strong technology, innovative R&D, and in-house automation, DelSolar has successfully developed a new series of cells with conversion efficiencies of 18.3% for mono-crystalline and 16.6% for multi-crystalline silicon cells. This industry-leading achievement is scheduled for volume production in Q3 this year.
In addition to high-efficiency, the new cells also feature a low temperature coefficient, less light-induced degradation, minimal module hot spot risk, and provide an extra premium to module and system customers with their high power output.